How to control ADAS3022?

I am using EVAL-ADAS3022EDZ in order to perform a data acquisition (for any input, just the first test). But the ADAS3022 Evaluation Software does not permit to change the parameters I need to change.

I would like to find an alternative way to perform a data acquisition changing the throughput value, analyzing more than one input, in a different time scale, etc.

Is there any possibility to use functions and control the data acquisition in a personalized way?

Thanks

Parents
  • Hi,

    The aim is to test the ADAS3022 using multiple inputs at the same time, using a personalized throughput, setting different PGIA for each input and plotting all of them in the same graph, where I could set the horizontal span to samples/time. However, the evaluation software just allows me to plot one input at the same time, with the same PGIA for all of them, etc.

    Regards,

    Marcel

Reply
  • Hi,

    The aim is to test the ADAS3022 using multiple inputs at the same time, using a personalized throughput, setting different PGIA for each input and plotting all of them in the same graph, where I could set the horizontal span to samples/time. However, the evaluation software just allows me to plot one input at the same time, with the same PGIA for all of them, etc.

    Regards,

    Marcel

Children
No Data