Post Go back to editing

AD7746 Calibration

Thread Summary

The user is experiencing issues with offset calibration on the AD7746, where the offset registers always show zeros after calibration. The support engineer confirmed that the offset calibration register is reloaded with the default value (0x8000) at power-on or reset, and suggested checking communication with the part and trying the CAPDAC for larger offset values. The user confirmed they could write to other registers and tried measuring parasitic capacitance without success, indicating a potential issue with the circuit inside the chip.
AI Generated Content

I am working on a circuit design with AD7746. Now I am facing a problem is about the offset calibration. I write the register into calibration mode and when the calibration is done, the offset registers always shows zeros, like having never been calibrated. I also has an EVL-board, its calibration works well. Is that wrong to do calibration with connecting the capacitor? Or there is something special design in EVL-board?