Post Go back to editing

AD7746 Calibration

Thread Summary

The user is experiencing issues with offset calibration on the AD7746, where the offset registers always show zeros after calibration. The support engineer confirmed that the offset calibration register is reloaded with the default value (0x8000) at power-on or reset, and suggested checking communication with the part and trying the CAPDAC for larger offset values. The user confirmed they could write to other registers and tried measuring parasitic capacitance without success, indicating a potential issue with the circuit inside the chip.
AI Generated Content

I am working on a circuit design with AD7746. Now I am facing a problem is about the offset calibration. I write the register into calibration mode and when the calibration is done, the offset registers always shows zeros, like having never been calibrated. I also has an EVL-board, its calibration works well. Is that wrong to do calibration with connecting the capacitor? Or there is something special design in EVL-board?

Parents
  • Hi, Eric

    Thank you for your replying. I am certainly sure about the offset calibration function works, and I could write the register correctly. But the problem is whatever I did with the circuit (open loop, short, with cap, etc), the calibration returns the same 0x8000 as you said, which means zeros. I have tried to use LCR measure the parasitic cap on the board, but it can't give out a value from CIN and EXC. It caused by circuit inside the chip. I am going to try CAPDAC by your advice.

    Thanks,

    Ye

Reply
  • Hi, Eric

    Thank you for your replying. I am certainly sure about the offset calibration function works, and I could write the register correctly. But the problem is whatever I did with the circuit (open loop, short, with cap, etc), the calibration returns the same 0x8000 as you said, which means zeros. I have tried to use LCR measure the parasitic cap on the board, but it can't give out a value from CIN and EXC. It caused by circuit inside the chip. I am going to try CAPDAC by your advice.

    Thanks,

    Ye

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.