AD7655 relationship between internal MUX and accuracy

Hello

Our customer is measuring accuracy of AD7655 and please let me know your advice relationship between internal MUX and accuracy.

Our test resul shows  large difference  (about 50~100LSB) between channel A (INA1 and INA2) and channle B (INB1 and INB2).

So, he has verified as below .

Input: AGND

Power supply: 5V

REF: AD1582

Interface: test  using both SPI and parallel

Number of test: 500  ( test is 2pattern which remains A0 = low  or high )

Sample: 3 samples

Test  result is below

Channle A (IINA1 and INA2) : about  100LSB +- 10LSB

Channle B (INB1 and INB2) :almost 0LSB

( for your information,  

in the case of input 1.0V ,  ( output of ADA4666-2 voltage follower is connected to INA1, INA2 , INB1 and INB2) ,

channle A  = 13296LSB (averaged value for 500 time),

channelB = 13230LSB (averaged value for 500 times)

I think that the internal difference between Channel A and B is internal MUX of AD7655.

Does internal MUX affect converted result as above  ?

I would like to know if above appearance is in specifaication or AD7655 characteristcs .

And we are checking his circuit design , layout and timing diagram.

Please let me know your advice

Regards,

Terumasa


Parents
  • 0
    •  Analog Employees 
    on Jan 8, 2016 7:21 PM

    Hello Terumasa,

    The AD7655 has a gain error specification of +/- 0.5% FSR.  This corresponds to +/-327 LSB.  The worst case would be where channel A has a +327 LSB gain error and channel B has -327 LSB gain error or vice versa.  In this case, you could expect upwards of a 650 LSB difference between A and B with a full-scale input.  However, this would be worst case. A typical device should have a gain error about half this much.  This only accounts for the gain error.  One would also have to factor in the offset error to get the expected value of a given input voltage.

    With that being said, it's always a good idea to minimize the resistance on the reference node.  This node must be able to properly regulate the reference load.  Any unperceived change in the reference value will manifest as a gain error.  Given the average reference current draw of 180 uA, the output resistance of the reference source must be kept to less than 200 mOhms to properly regulate the reference current assuming a 2.5 V reference is utilized.

    -- Ryan

Reply
  • 0
    •  Analog Employees 
    on Jan 8, 2016 7:21 PM

    Hello Terumasa,

    The AD7655 has a gain error specification of +/- 0.5% FSR.  This corresponds to +/-327 LSB.  The worst case would be where channel A has a +327 LSB gain error and channel B has -327 LSB gain error or vice versa.  In this case, you could expect upwards of a 650 LSB difference between A and B with a full-scale input.  However, this would be worst case. A typical device should have a gain error about half this much.  This only accounts for the gain error.  One would also have to factor in the offset error to get the expected value of a given input voltage.

    With that being said, it's always a good idea to minimize the resistance on the reference node.  This node must be able to properly regulate the reference load.  Any unperceived change in the reference value will manifest as a gain error.  Given the average reference current draw of 180 uA, the output resistance of the reference source must be kept to less than 200 mOhms to properly regulate the reference current assuming a 2.5 V reference is utilized.

    -- Ryan

Children
No Data