AD7984 module fails to measure voltage below 2.5 V

I have tested several of these modules, each of them failed after a while and reports any value below 2.5 V (2.5 to -5 V) as 0. To my surprise, it seems to happen whenever the PMOD connection stops to provide voltage (3.3V and GND) while the voltage -2.5V, 0, 7.5 are still on.

I have also found funny little "note" in the schematic file "Ensure 'we' power the ADC up after Pmod Controller board" (just floating piece of text on the 2nd page of schematic file).

I am not sure who the above mentioned 'we' are,  perhaps bunch of analog device engineers.

Anyway, could someone prove me right that the module fails to operate properly, once it is subjected to above mentioned situation ? If so, could someone give an explanation, why is this board advertised as plug-in, stand-alone evaluation board, when it misses any documentation, sample design and requires external voltage source ?

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:27 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:27 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data