Post Go back to editing

AD7915 - Connection of VDD bypass caps to AGND or DGND?

Thread Summary

The user asked about the proper connection of bypass capacitors for the VDD pin (2.5V power rail for ADC core) in the AD7915 when using separate AGND and DGND ground planes. The final answer indicates that the VDD bypass capacitors should be connected to AGND to minimize high-frequency noise interference, as outlined in the user guide UG-340. The pin layout, with VDD adjacent to the analog input pins, supports this configuration.
AI Generated Content

From customer:

I am planning to have independent AGND and DGND ground planes in my system, and plan to short the two GNDs together at or under the ADC.

If I use the AD7915, would the bypass capacitors for VDD (2.5V power rail for ADC core) be connected to AGND or DGND?

Initially I would have thought it would attach to DGND, since it drives the ADC SAR structures and likely has some high-frequency digital content.

But I noticed in one of the packages that the VDD pin is placed right next to the analog IN+/- pins, and I know the pin layouts on these ADCs is derived to allow a AGND/DGND split across the part body center. This seems to imply that it would be better to bypass VDD to AGND…