AD7173-8 and multiple channel sampling

Hi everyone, I am trying to use AD7173-8 in an application where 3 channels are to be used and I am a little confused about that.

In particular:

  • The AD7173-8 is connected to a microcontroller via SPI. I have configured SPI according to the datasheet and communications are OK. The SPI clock frequency that I am currently using for tests is 2 MHz and I intend to push it further, if necessary. Data read from the ADC are seen on the DOUT/~RDY pin of the ADC.
  • ADC configuration details:
    • Only 3 channels of the ADC are enabled; the rest are disabled on power-up.
    • ADC MODE:SING_CYC bit is set, mode: continuous conversion, delay after channel switch: 0 us
    • IF MODE / DATA STAT: enabled for testing
    • Two setups are used (0 and 1); in setup 0, output is offset binary and in setup 1 output is unipolar.
    • Two filter configurations are used (0 and 1); in FILTCON0, sinc5+sinc1 is used and ODR is 10417 samples/s - in FILTCON1, sinc3 is used and ODR is 20.01 samples/s (this is for sampling a temperature sensor output that does not change fast)
    • External reference (ADR4533, +3.3 V) is used and external buffers (AD8572) are placed between analog voltages and ADC, thus input buffers are disabled; clock is provided by an external crystal at 16 MHz
  • The microcontroller reads the data register of the ADC at regular time intervals (upon overflow of a timer).
  • Having only one channel enabled, everything works OK. I can read data into the microcontroller's registers and they correspond to the known analog voltage values that are present each time. I read 3+1 = 4 bytes (3 with data and 1 with the contents of the STAT register).
  • When I try to enable two channels, I read 2x(3+1) = 8 bytes that correspond to successive readings of the data register. I notice that, when stepping through the microcontroller's code, the first 4 bytes correspond to one of the two ADC channels and the remaining 4 are rubbish (0xFFs); however, the STAT register contents indicate that sometimes one channel is read, sometimes the other.

What I want to do is to have a consistent way of reading all enabled channels of the ADC. The datasheet says about the DOUT/~RDY pin that goes low to indicate that a conversion has been completed. Up to now, when hooking a 'scope to check logic levels on the SPI lines, I cannot see DOUT/~RDY going low right after an SPI transaction; it remains high and then it goes Hi-Z (green trace is ~CS, yellow trace is DOUT/~RDY):

Has anyone a suggestion to move forward? What exactly should I have to do to switch channels fast enough without losing data?

Parents
  • 0
    •  Analog Employees 
    on Jun 23, 2016 7:02 PM over 4 years ago

    Hi,

    1. In continuous conversion mode, the ADC converts continuously and when /CS is low the DOUT/RDY pin goes low each time a conversion is complete. So it is really important to monitor the DOUT/RDY pin or the /RDY bit in the status register and start reading the conversion as soon as it goes low. The /RDY pin is reset high when a read operation is complete and remains high until the next conversion is complete.

    2. Yes, sufficient number of SCLKs must be provided and the SCLK rate must be fast enough so that a read is completed before the next conversion result and to avoid losing data.

    3. When several channels are enabled, the ADC automatically sequences and performs conversion through the enabled channels. But then again, the DOUT/RDY pin pulses low each time the conversion is complete. So, just like the thread that you have mentioned you can monitor the DOUT/RDY pin and use it as an interrupt to the microcontroller to read a conversion result. 

    Thanks,

    Jellenie

Reply
  • 0
    •  Analog Employees 
    on Jun 23, 2016 7:02 PM over 4 years ago

    Hi,

    1. In continuous conversion mode, the ADC converts continuously and when /CS is low the DOUT/RDY pin goes low each time a conversion is complete. So it is really important to monitor the DOUT/RDY pin or the /RDY bit in the status register and start reading the conversion as soon as it goes low. The /RDY pin is reset high when a read operation is complete and remains high until the next conversion is complete.

    2. Yes, sufficient number of SCLKs must be provided and the SCLK rate must be fast enough so that a read is completed before the next conversion result and to avoid losing data.

    3. When several channels are enabled, the ADC automatically sequences and performs conversion through the enabled channels. But then again, the DOUT/RDY pin pulses low each time the conversion is complete. So, just like the thread that you have mentioned you can monitor the DOUT/RDY pin and use it as an interrupt to the microcontroller to read a conversion result. 

    Thanks,

    Jellenie

Children
No Data