Post Go back to editing

AD7323 output deviation with SPI frequency?

Currently we use AD7323 ADC with;

Vdd=12V,

Vss=gnd,

Vcc=3.3V,

Vref=3V

and moving average over 16 samples.

In case of 5Mhz SPI interface case we got the following results with straight binary coding;

Input Output
0 0
1 0.99
2 1.99
3 3.0
4 4.0
5 5.0
6 5.92
7 6.74
8 7.57
9 8.41
10 9.26

As it is seen above 5V input case all results deviate from the input. If we decrease SPI frequency to 1MHz (our trial frequecny) all results turned back to normal.

Do you have any idea or feedback what could be the reason of this deviation?

Regards