5V voltage reference for the AD7718?

My application requires converting voltages from (almost) 0 to 5V using fully differential probing. From the application sheet it seems like I need to use a 2.5V reference in order to cover the entire input range of the ADC?

Somehow it seems that in order to run the setup I need want RN2 = RN1 = RN0 = 1 in ADCCON & Vref2 = 2.5V & Vredf1 = GND (0V). Is this correct?

Parents
  • 0
    •  Analog Employees 
    on Sep 25, 2016 7:12 PM

    Hi,

    The nominal reference voltage for specified operation, VREF, (REFIN1(+)–REFIN1(–) or REFIN2(+)–REFIN2(–)), is 2.5 V, but the AD7708/AD7718 is functional with reference voltages from 1 V to AVDD. With Vref = 2.5V, the part allows to handle unipolar analog input ranges from 0 mV to +20 mV to 0 V to +2.5 V and bipolar inputs of +/-20 mV to +/-2.5 V. Because the part operates from a single supply these bipolar ranges are with respect to a biased-up differential input. Meaning, if you want to measure an input voltage range of 0 to 5V, you have to operate in pseudo-differential mode  referenced to AINCOM = 2.5V. If AINCOM is 2.5 V and the AD7718 is configured for an analog input range of +/-2.56 V, the analog input range on the AIN1 input can cover 0V to 5V (i.e., 2.5 V +/-2.56V). Bipolar or unipolar options are chosen by programming U/B bit in the ADCCON register.

    Thanks,

    Jellenie

  • 你好,今天看到了这个帖子,AD7708/ad7718如果要测量0至5V的输入电压范围,只能在伪差分模式下工作吗?在全差分模式下,可以吗?比如,AIN1/AIN2,将AIN2接上2.5V?

    谢谢,期待你的回答

  • 0
    •  Analog Employees 
    on Dec 17, 2019 3:04 AM in reply to tsxyzyb

    Hi,

    EngineerZone (ez.analog.com) offers support for English language inquiries only. Please post your question in English so that all members can read it. If you require assistance in Chinese please visit https://ez.analog.com/cn.

    Thanks,

Reply Children
No Data