5V voltage reference for the AD7718?

My application requires converting voltages from (almost) 0 to 5V using fully differential probing. From the application sheet it seems like I need to use a 2.5V reference in order to cover the entire input range of the ADC?

Somehow it seems that in order to run the setup I need want RN2 = RN1 = RN0 = 1 in ADCCON & Vref2 = 2.5V & Vredf1 = GND (0V). Is this correct?

Parents
  • 0
    •  Analog Employees 
    on Sep 25, 2016 7:12 PM

    Hi,

    The nominal reference voltage for specified operation, VREF, (REFIN1(+)–REFIN1(–) or REFIN2(+)–REFIN2(–)), is 2.5 V, but the AD7708/AD7718 is functional with reference voltages from 1 V to AVDD. With Vref = 2.5V, the part allows to handle unipolar analog input ranges from 0 mV to +20 mV to 0 V to +2.5 V and bipolar inputs of +/-20 mV to +/-2.5 V. Because the part operates from a single supply these bipolar ranges are with respect to a biased-up differential input. Meaning, if you want to measure an input voltage range of 0 to 5V, you have to operate in pseudo-differential mode  referenced to AINCOM = 2.5V. If AINCOM is 2.5 V and the AD7718 is configured for an analog input range of +/-2.56 V, the analog input range on the AIN1 input can cover 0V to 5V (i.e., 2.5 V +/-2.56V). Bipolar or unipolar options are chosen by programming U/B bit in the ADCCON register.

    Thanks,

    Jellenie

  • 你好,今天看到了这个帖子,AD7708/ad7718如果要测量0至5V的输入电压范围,只能在伪差分模式下工作吗?在全差分模式下,可以吗?比如,AIN1/AIN2,将AIN2接上2.5V?

    谢谢,期待你的回答

Reply Children