Post Go back to editing

The imput impedance of AD7124-8

Thread Summary

The user inquired about the input impedance of the AD7124-8, which is not directly specified in the datasheet. The input current is provided instead: +/-1nA for low power mode, +/-1.2nA for mid power mode, and +/-3.3nA for full power mode when buffered. For unbuffered operation, the input current is +/-2.65uA/V. The input buffers are automatically enabled for Gain > 1, allowing the device to handle significant source impedances.
AI Generated Content

Hi,

Could anyone tell me what the imput impedance of AD7124-8 would be?

I could not find any infomation about it on its data sheets.

Thanks!

  • Hi,

    We list the input current specification rather than specify the input impedance. The input impedance can be calculated from this input current specification. When buffer is enabled, the absolute input current is +/-1nA for low power mode, +/-1.2nA for mid power mode and +/-3.3nA for full power mode. With Gain > 1, the input buffers are automatically enabled. Thus, it can handle any significant source impedances which allows external filtering necessary in your application. When, un-buffered the absolute input current is +/-2.65uA/V. These values can be found in datasheet specification section.  

    Thanks,

    Jellenie

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin