Post Go back to editing

AD7091R使用咨询

使用AD8275和AD7091R-4BCPZ-RL7设计4路ADC采集电路上报给CPLD

1.在测量0~10V输入时,AD8275的ref1和ref2接GND,AD7091R的ref接2.048V

2.在测量-12V~+12V输入时,AD8275的ref1和ref2接2.5V,AD7091R的ref接5V(ref191更换为ref195)

问题:

1.使用1片ref192是否可以满足4片AD8275的参考电压的电流需求?

2.AD7091R的muxout直连ADCin在PCB布线上是否有屏蔽要求?什么情况需要增加filter?

3.AD7091R的SDO是否需要加47K上拉?其他SPI管脚是否有上下拉要求?

4.convst、reset、cs是否需要10k上拉?