Post Go back to editing

Questions about AD7172/5/7-2

I have questions about AD7175-2, but I beleive they would also valid for AD7172-2 and AD7177-2, so the answers would be relevant for their users too.

  1. May the inputs be shared between the channels? E. g if Ain0 and Ain1 set up for differntial measurement on channel 0, may the Ain1 be used for single ended measurement on channel 1?
  2. I am a bit confused about dat rate and channels. if the data rate is 100 SPS, would it mean 50 SPS effective rate with 2 channels?
  3. For the reason of simplicity the ADC is to be used to measure following signals with full scale voltages:
  1.  +/- 1 V bipolar differential signal. (eg channel 0) 
  2. 5 V unipolar pseudodifferintal (channel 1)

The b) forces to use 5 V external refernce, which is disadvantageous for measurement on channel 1. Luckily, the ADC has inetrnal 2.5 V reference, which could be used on channel 1 to bring it closer to optimum range. Would it make sense to do so?

I may have further questions as I move on with the programming.

Parents
  • 4. What is current to the input, if it is not connected to a sampling channel (multiplexer us open)?

    5. Assume I make a psudo differntial measurement mentioned in question 3b. The Ain+ connected to the signal and Ain- normally to the ground. What happens if the voltage on Ain- sinks below 0 V due to a disturbance?

Reply
  • 4. What is current to the input, if it is not connected to a sampling channel (multiplexer us open)?

    5. Assume I make a psudo differntial measurement mentioned in question 3b. The Ain+ connected to the signal and Ain- normally to the ground. What happens if the voltage on Ain- sinks below 0 V due to a disturbance?

Children
No Data