Confirm whether we can use AD574ASD/883B in the design

@

Hi,

We have selected part AD574ASD/883B (ADC Single SAR 12-bit Parallel 28-Pin SBCDIP).

In Analog Devices website it is showing that all the parts of family AD574ASD are NRND (Not Recommended For New Design).

Please confirm whether I can go ahead with the part AD574ASD/883B, Is there any difficulty in procurement and getting future technical supports during functionality testing If I choose this part.

Regards,

  • People want faster, more bits, and smaller packages, so more and more ADCs are serial.  However,

    you could look at the AD676, AD1674, or AD7880.   If you want an AD574, you will have to buy

    the 5962xxxx full mil part.

    Harry

  • Hi Vijetha,

       I agree with what Harry is saying. Now we wanted to help in the development of your application. The AD574 is a good part. ADI has newer parts that can fit your application and many of them are of industrial standard. Do you have specifics about ad574 why you chose it? In your application of a temperature monitoring system a more accurate would be better and this can be achieve when you have a higher resolution ADC and very good parametric specification. In your application, what is the range of temperature that you are monitoring? What accuracy does it need? Here is a link of the ADC that may fit your application, I have filter it to 1 channel, parallel interface and covers industrial temperature range. Please refer to the link. You may also want to filter further the list base from the specification that you need. If you have questions, please let us know.

    http://www.analog.com/en/parametricsearch/10825#/p1746=16.6|10000000&p4364=Sigma-Delta|SAR&p2846=-40%20to%20125%B0C|-40%20to%20105%B0C|-40%20to%2085%B0C&p4365=Parallel&p3062=1&ps5=select%20all

    Regards,

    Jonathan

  • 5962R8512701VXA

    http://www.analog.com/en/products/application-specific/militaryaerospace/aerospace/ad574s.html#product-samplebuy 

    As a side note, NRFD does NOT mean the part is going obsolete;  it simply means that it is a mature product,

    and there are newer parts that you should consider.  For example, more bits, faster, lower cost because they

    are on a newer process, etc.  But if the rest of the world is designing in the newer parts, and the existing

    customers drop off one by one, eventually it will be announced for obsolescence, it which case we give you

    one year for your final buy.

    Harry

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin