KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
AD7683
Production
The AD7683 is a 16-bit, charge redistribution, successive approximation, PulSAR® analog-to-digital converter (ADC) that operates from a single power supply...
Datasheet
AD7683 on Analog.com
ADR435
Production
The ADR430/ADR431/ADR433/ADR434/ADR435 series is a family of XFET® voltage references featuring low noise, high accuracy, and low temperature drift performance...
Datasheet
ADR435 on Analog.com
Hi,
I am interesting to use TL431 voltage reference to generate 5V to be used in Vref input of AD7683.
This voltage reference has low noise voltage enough for AD7683?
I am asking because many voltage reference devices inform noise voltage parameter, normally in a specific range of frequency and in micro volts.
For example, ADR435 device, from Analog: Low noise (0.1 Hz to 10.0 Hz): 3.5 µV p-p @ 2.5 V output.
Unfortunatelly, this information does not informed in the TL431 datasheet. I tried TI, OnSemi, etc...
Regards,