KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD7683
Production
The AD7683 is a 16-bit, charge redistribution, successive approximation, PulSAR® analog-to-digital converter (ADC) that operates from a single power supply...
Datasheet
AD7683 on Analog.com
ADR435
Production
The ADR430/ADR431/ADR433/ADR434/ADR435 series is a family of XFET® voltage references featuring low noise, high accuracy, and low temperature drift performance...
Datasheet
ADR435 on Analog.com
Hi,
I am interesting to use TL431 voltage reference to generate 5V to be used in Vref input of AD7683.
This voltage reference has low noise voltage enough for AD7683?
I am asking because many voltage reference devices inform noise voltage parameter, normally in a specific range of frequency and in micro volts.
For example, ADR435 device, from Analog: Low noise (0.1 Hz to 10.0 Hz): 3.5 µV p-p @ 2.5 V output.
Unfortunatelly, this information does not informed in the TL431 datasheet. I tried TI, OnSemi, etc...
Regards,
I would not even consider the TL431 with a 16 bit ADC; you are just throwing money away.
The TL431 is a commodity reference, with 50 ppm/C tempco. So after your temperature
changes by 10 degrees, you have less than a 14 bit system. There is a noise curve
(fig 7) on the TI data sheet. Integrate over your bandwidth.
Depending on system cost target, look at the ADR3425 or the ADR4525 and everything
in between.
Harry
I would not even consider the TL431 with a 16 bit ADC; you are just throwing money away.
The TL431 is a commodity reference, with 50 ppm/C tempco. So after your temperature
changes by 10 degrees, you have less than a 14 bit system. There is a noise curve
(fig 7) on the TI data sheet. Integrate over your bandwidth.
Depending on system cost target, look at the ADR3425 or the ADR4525 and everything
in between.
Harry