KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD7683
Production
The AD7683 is a 16-bit, charge redistribution, successive approximation, PulSAR® analog-to-digital converter (ADC) that operates from a single power supply...
Datasheet
AD7683 on Analog.com
ADR435
Production
The ADR430/ADR431/ADR433/ADR434/ADR435 series is a family of XFET® voltage references featuring low noise, high accuracy, and low temperature drift performance...
Datasheet
ADR435 on Analog.com
Hi,
I am interesting to use TL431 voltage reference to generate 5V to be used in Vref input of AD7683.
This voltage reference has low noise voltage enough for AD7683?
I am asking because many voltage reference devices inform noise voltage parameter, normally in a specific range of frequency and in micro volts.
For example, ADR435 device, from Analog: Low noise (0.1 Hz to 10.0 Hz): 3.5 µV p-p @ 2.5 V output.
Unfortunatelly, this information does not informed in the TL431 datasheet. I tried TI, OnSemi, etc...
Regards,
I would not even consider the TL431 with a 16 bit ADC; you are just throwing money away.
The TL431 is a commodity reference, with 50 ppm/C tempco. So after your temperature
changes by 10 degrees, you have less than a 14 bit system. There is a noise curve
(fig 7) on the TI data sheet. Integrate over your bandwidth.
Depending on system cost target, look at the ADR3425 or the ADR4525 and everything
in between.
Harry