AD7091R-4 Malfunctioning

Hi,

 

I am validating a design using a AD7091R-4 ADC and some errors are coming up. This component has been used in 12 boards, and all 12 of them are showing the same problem. Might it be due to a faulty batch?

 

When the system is turned ON it might happen that the ADC works correctly or it starts outputting wrong values and transitioning to wrong channels, and won't stop failing, this error sometimes is fixed when rebooted.

 

The ADC is routed as shown below, and when is working properly outputs the data shown in the next figure. Which correspond to the ADC working in normal operation, with channels 0,1 & 2 selected, followed by the value of configuration and channel registers.

When it boots failing, the output is as shown below . Sometimes the channel sequence is correct , but the values never are in all three. The value is allways right in channel 0 (reference voltage), and sometimes in channel 2, but hardly ever in channel 1. Even the configuration and channel registers output a wrong value sometimes.

A SW reset is performed at boot time with 66 convst pulses,  then write in every register, set the sw reset bit, and then read all the registers (shown below).

Any ideas why it might show this behaviour? 

Thank you in advance

Parents
  • 0
    •  Analog Employees 
    on Aug 31, 2017 2:37 PM

    Hello Husein and all

    I'm debugging this same part for a customer, it may be a bit late, if you don't mind I post it here so others may benefit from this thread.

    As far as I'm aware, there is no issues with the part or batch numbers. The Reset pin needs to be properly control.

    From your schematic the reset pin is permanently tie high via a resistor !.  Ideally it should  also be tied to a microprocessor where it can issues a reset in the form of a pulse (i.e. high-Low-high) in order to reset the IC just after power-up. 
    The reset 'pulse width' and the reset 'pulse delay' should comply to our specification. see fig. 43 and Table 2, of the AD7091R-4 Data Sheet Rev.C.
     

    After the power up and reset it by pulsing it, from here you may use the soft reset (SRST) see table 16. Please note using this Software reset function will resets the internal digital control logic and the result and alert registers, but it does not reset the other memory map registers.

     

    Alternatively as your hardware stands, your only option now is to use the power-on devices initialization method as described in page 33 of the data sheet Rev.C. which you are trying to do from your plots. However from looking at your convst signal graph it appears half a cycle out.  The Convst signal should be default high at all times and should pulse as and when required from high-low-high. Try default high your Convst signal at all times unless starting to pulse it.

    Also if  you start the Convst signal low and then pulsing it,  in order to start a conversion please note your half cycle out (delayed) as the Convert Start Input Signal is Edge triggered logic input. The falling edge of CONVST places the track-
    and-hold mode into hold mode and initiates a conversion.

     

    Great if you can send me a higher resolution of the above screenshots and a Convst signal for a start convert case.

     

    Regards,

    Ching

Reply
  • 0
    •  Analog Employees 
    on Aug 31, 2017 2:37 PM

    Hello Husein and all

    I'm debugging this same part for a customer, it may be a bit late, if you don't mind I post it here so others may benefit from this thread.

    As far as I'm aware, there is no issues with the part or batch numbers. The Reset pin needs to be properly control.

    From your schematic the reset pin is permanently tie high via a resistor !.  Ideally it should  also be tied to a microprocessor where it can issues a reset in the form of a pulse (i.e. high-Low-high) in order to reset the IC just after power-up. 
    The reset 'pulse width' and the reset 'pulse delay' should comply to our specification. see fig. 43 and Table 2, of the AD7091R-4 Data Sheet Rev.C.
     

    After the power up and reset it by pulsing it, from here you may use the soft reset (SRST) see table 16. Please note using this Software reset function will resets the internal digital control logic and the result and alert registers, but it does not reset the other memory map registers.

     

    Alternatively as your hardware stands, your only option now is to use the power-on devices initialization method as described in page 33 of the data sheet Rev.C. which you are trying to do from your plots. However from looking at your convst signal graph it appears half a cycle out.  The Convst signal should be default high at all times and should pulse as and when required from high-low-high. Try default high your Convst signal at all times unless starting to pulse it.

    Also if  you start the Convst signal low and then pulsing it,  in order to start a conversion please note your half cycle out (delayed) as the Convert Start Input Signal is Edge triggered logic input. The falling edge of CONVST places the track-
    and-hold mode into hold mode and initiates a conversion.

     

    Great if you can send me a higher resolution of the above screenshots and a Convst signal for a start convert case.

     

    Regards,

    Ching

Children
No Data