AD7367 Evaluation board

I need information about the AD7367 evaluation board. According to the datasheet the board includes a level shifter to translate the communication signals from 3.3V to 5V. Using that level shifter, is it possible to use the SPI at 48 MHz even if the board is connected to devices with a 3.3V logic? Or the maximum frequency is limited to 35 MHz.

Best regards.

Parents Reply Children
No Data