ADAS3022 Recommended Circuit Help

I see in the Recommended circuit schematic for the ADAS3022 ADC that the ADR434 is to be used for providing the 4.096 V reference voltage. When I considered the ADR434 datasheet, I see that it is meant to operate at a voltage from 6V-18V. The Recommended circuit for the ADAS3022 designates that a 5V input should be given to the ADR434. Is this correct? If not, how can the circuit be adjusted to consider this? Any assistance would be appreciated.

Parents
  • Hi codigwe,

    Seems you follow the recommended setting for the reference circuit.It should be able to power the ADR435 with a  +15V supply. . Aside from ADAS3022 and ADR435 what other components connected to this? it draw current if the total impedance excess  than  expected. I should check first the  power supply circuit.Try to limit the connection on this. Please take note ADP1612/13 as per datasheet page3 Vout=12V  ILoad is limited to 10mA to 150mA.

    regards,

    LLoben

Reply
  • Hi codigwe,

    Seems you follow the recommended setting for the reference circuit.It should be able to power the ADR435 with a  +15V supply. . Aside from ADAS3022 and ADR435 what other components connected to this? it draw current if the total impedance excess  than  expected. I should check first the  power supply circuit.Try to limit the connection on this. Please take note ADP1612/13 as per datasheet page3 Vout=12V  ILoad is limited to 10mA to 150mA.

    regards,

    LLoben

Children
No Data