ADAS3022 Recommended Circuit Help

I see in the Recommended circuit schematic for the ADAS3022 ADC that the ADR434 is to be used for providing the 4.096 V reference voltage. When I considered the ADR434 datasheet, I see that it is meant to operate at a voltage from 6V-18V. The Recommended circuit for the ADAS3022 designates that a 5V input should be given to the ADR434. Is this correct? If not, how can the circuit be adjusted to consider this? Any assistance would be appreciated.

Parents Reply Children
No Data