Post Go back to editing

ADAS3022 Recommended Circuit Help

I see in the Recommended circuit schematic for the ADAS3022 ADC that the ADR434 is to be used for providing the 4.096 V reference voltage. When I considered the ADR434 datasheet, I see that it is meant to operate at a voltage from 6V-18V. The Recommended circuit for the ADAS3022 designates that a 5V input should be given to the ADR434. Is this correct? If not, how can the circuit be adjusted to consider this? Any assistance would be appreciated.

Parents
  • Dear LLoben,

    Thank you very much for your reply. Would this mean that I should be able to power the ADR434 with the +15 V rail and keep all of the other connections in the recommended circuit the same? I have tried this, and I am experiencing strange behavior with the circuit drawing up to 200 mA in current without the ADAS3022 being operational. Please let me know of any changes that can correct this problem.

Reply
  • Dear LLoben,

    Thank you very much for your reply. Would this mean that I should be able to power the ADR434 with the +15 V rail and keep all of the other connections in the recommended circuit the same? I have tried this, and I am experiencing strange behavior with the circuit drawing up to 200 mA in current without the ADAS3022 being operational. Please let me know of any changes that can correct this problem.

Children
No Data