I see in the Recommended circuit schematic for the ADAS3022 ADC that the ADR434 is to be used for providing the 4.096 V reference voltage. When I considered the ADR434 datasheet, I see that it is meant to operate at a voltage from 6V-18V. The Recommended circuit for the ADAS3022 designates that a 5V input should be given to the ADR434. Is this correct? If not, how can the circuit be adjusted to consider this? Any assistance would be appreciated.