Post Go back to editing

AD4007 / AD4003 - TIA interface

Hello,

we are looking into a transimpedance amplifier frontend based on the AD8597 for the AD4007 (or the AD4003).

Is it feasible to use the AD8597 as a buffer for the SAR ADC ?

Would there be any drawbacks compared to the suggested ADA4897 in the datasheet of the AD4007 as an input buffer ?

Is a two stage TIA design (TIA with second stage buffer) mandatory - or could a single stage TIA - consisting of the AD8597 be sufficient ?

What would be a recommmended way to adapt the TIA to the (fully) differential interface ?

Does it make sense to implement a fuly differential TIA or is there a pseudo differential input feasible as it could be done for Linear's LTC2368 ?

Best, Thorsten

  • Hi Thorsten,

    I'm looking into this and get back to you asap.

    regards,

    LLoben

  • Hi Thorsten,

    I'd like to get more information about your application.What's driving the need(performance- SNR/THD, Linearity?) to use a differential SAR ADC?.What is your input signal bandwidth. I presume its below 100Hz. Although we haven't verified the AD400x family performance with AD8597 as a driver,it should still be able to drive the AD4000/03/07 and achieve decent performance for low frequency input signal(<=100Hz) with High-Z mode enabled. I'd suggest you to use the ADA4940 as a single-ended to differential driver between the AD8597 and AD4003/07. The AD400x eval board (user guide) has a footprint for the AD4940,which will allow you to evaluate the performance for this signal chain.See this article if it helps. Unlike traditional SAR ADCs, a unique combination of high-input impedance mode,reduced input current and longer acquisition phase reduces the settling requirements on the ADC driver and hence a higher noise and /or lower power/bandwidth amplifier can be used.

    regards,

    LLoben

  • Thank you for the feedback, LLoben !

    The application basically is scanning with a step frequency of 200kHz. The settlement time of the stimulus (input of the photodiode) is pretty fast (<300ns). For the photodiode/TIA side simulation/calculation based on the AD8597 let me expect that we will achieve a settlement time to <0.01% of less than 3us. Within the 5us timing window (because of the 200kHz scanning frequency) there is enough time left after settlement for conversion with a SAR ADC like the AD4007.

    Based on a two stage TIA-configuration with the AD8597 for a photodiode current of 1mA an SNR towards 100dB is achievable - which corresponds well to the achievable SNR of the ADC and the requirements of at least 92dB SNR.

    Hope this gives at least a short intro to the boundary conditions of the application.

    If there should be questions please let me know ...

    As you said you would assume a "decent" performance of the AD8597 with the AD4007 at signal frequencies of about 100Hz - my question would be : What is your assumption with regard to the application case described above -obviously thew performance requitrements are "slightly" different ...  My assumption that directed me towards the AD4007 was that because of the High-Z-Mode it should be "easy" for the AD8597 to settle in the available time... How is your perception ?

    Thx for the hint towards the AD4940 - I will look into a combination with the AD8597 as a TIA ...

    Best, Thorsten

  • Hi Thorsten,

    Have you looked at Analog Devices photo diode tool for this TIA configuration?

    http://www.analog.com/designtools/en/photodiode/

     

    The AD8597 should be able to achieve decent performance based on its datasheet specs (10MHz GBP, 1.1 nV/Hz noise) and what we have seen with other precision amplifiers (See figures 45 and 46 in datasheet) with High-Z enabled. However, I’d encourage you to evaluate this signal chain performance to make sure it meets your requirements.

    Regards,

    LLoben

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.