AD7091R-8 problem

hi every one,

I have problem to run AD7091R-8, I use fpga to use this ADC but when I initialize the ADC and set the registers and then I want to read back the registers to verify them. but there is no signal in SDO pin, I think maybe the IC didn't receive my command correctly I changed my code to send no command just do a convert and  then as it mentioned in the datasheet after get low the CS the IC will send converted data on the SDO automatically, but there is no signal on SDO pin yet. I will say the specification that I used to drive this IC please check it and help me to solve my problem.

*SCLK: 20MHz

*I send the data on the falling edge of the SCLK which the IC can receive it on the rising edge of the SCLK. is it right? IC will recieve data on the rising edge of the SCLK?

*as it mentioned in the datasheet the first data which is MSB bit will send out on the falling edge of CS and fpga will recive it on the first rising edge and the other bits will be send on the falling edge of SCLK and the fpga will receive them on the rising edge of the SCLK. is it right?

*I try hardware initialization and also software initialization  but none of them have solved my problem.

I attached the signals in the first picture I use software reset and as you see there is no signal on SDO and in the second picture I use hardware reset and as you see again there is no signal on the SDO pin.

thanks

Matin

attachments.zip
Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:55 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:55 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data