Post Go back to editing

I want to use AD7768 in daisy-chain mode with single serial (DOUT0) stream, e.g. FORMAT=11.  Which pin do I use to receive data from previous AD7768 in chain?  For the AD7768-4 it is clear (pin 21), but the data sheet is not so clear for the 8-ch

Thread Summary

The user asked about using a single DOUT on the AD7768. The final answer confirmed that pin 21 (DOUT6) should be used in this configuration. The issue with the previous reply being missing from public view is being addressed.
AI Generated Content

Hi John,

If you are using a single DOUT then you should also use pin 21 (DOUT6) on the AD7768. 

Regards

Niall

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
  • I have this answer too. Why do you not leave the answers available for other forum users?

  • Hi 

    Apologies for inconvenience. We are encountering some issue with the previous reply as it appears to be missing for public view but we are working on this so that others may be able to see this again. 

    Thanks,

    Jellenie 

  • Recovered the answer below.

    Hi John,

    If you are using a single DOUT then you should also use pin 21 (DOUT6) on the AD7768.

    Regards.