I am using AD7768 in PIN mode, I set the DECx and MODEx then apply a /RESET followed by a couple of /START to set the desired sampling rate and power mode (that seems to work OK), AVDDx=5.0V, IOVDD=3.3V, REF+ = 4.096V. My analog input range is approximately 2Vpp (centered on 2.5V offset), not the expected 8.192Vpp. I have the EVAL kit and it works as expected.