Good morning.
We are using AD7264 in our design.
AD7264 is interfaced with iMX6 NXP Processor.
We would be grateful to have any insight on the queries detailed.
Scenario:
Validating SPI Communication with AD7264
Queries
- Is there a specific initialisation sequence for AD7264?
- Does there exist a reference code for initialisation?
- Can internal registers be read from / written to without doing any calibration?
- Data is transferred to AD7264 in a packet of 8 bits. An idle period of 4.5 uSec is observed between two byte transfers. Will it affect SPI communication? (Please refer image AD7264_SCLK_TimeDelay.BMP)
- Is there a max. time delay acceptable between transfer of successive bytes?
- How critical are DIN setup time (3 nSec min.) and DIN hold time (3 nSec min.)? In our case, setup time is 0 and hold time is one SCLK cycle.
Steps carried out & observations:
- Read contents of ADC A Internal Offset Register after power-on.
(All "0" as suggested in datasheet Page # 23) - WRITE a known value (NOT CALIBRATION VALUE).
- Read contents of ADC A Internal Offset Register.
All "0". Expected is the written known value. - Carry-out (1) to (3) for
- ADC B Internal Offset Register
- ADC A External Gain Register
- ADC B External Gain Register
Results are the same as in case of ADC A Internal Offset Register.
Checks Performed
| Checks Performed | Observations |
|---|---|
| Chip select polarity | Idle high Active low during transmission |
| SCLK polarity | Idle high Active low during transmission |
| Chip select to SCLK setup time | 12 uSec Required is 10 nSec min. (Datasheet Page # 29) |
| SCLK frequency | 1 MHz |
| MOSI Data stream on AD7264 PD0/DIN pin | Expected data stream as per the WRITE / READ scenarios |
| MOSI data transfer w.r.t SCLK | Bits are transferred on "falling edge" of SCLK |
| AVcc | 5 V |
| Vdrive | 5 V |
| Vref | 2.5 external |
Bit Streams used
| Requirement | Bit stream |
|---|---|
| ADC A Internal Offset Reg. Read | (MSB) 0001 0010 0001 0001 0000 0000 0000 0000 (LSB) Last 20 LSBs are to generate SCLK for data receiving |
| ADC A Internal Offset Reg. Write | (MSB) 0010 0101 0101 0101 0000 (LSB) b15-b4 : dummy data 0x55 to validate read operation |
Best regards,
-- Utpal