Post Go back to editing

AD 7822 Confusing ~PD and ~CONVST

Good day everyone!

   I'm about to use AD 7822 but as I read the datasheet, I got confused regarding the ~PD and ~CONVST. The AD 7822 powers up (getting ready) if ~PD is logic high OR ~CONVST is logic high (after #ns of ~EOC duration). The word OR here confuses me.

1) If I tied ~PD permanently high to Vcc, does that mean the AD 7822 will not power down at all even if after ~EOC, ~CONVST is low? Is the state of ~CONVST ignored regarding power down if ~PD is always high?

2) Does that mean that a 1µs power up time will always be needed before every conversion start even if ~PD is tied to Vcc?

3) Can I use a continuous crystal oscillator (50/50) for ~CONVST, or does ~CONVST just accepts pulses or "per request" conversion? If yes, does that mean frequency of ~CONVST and sampling frequency is equal?

   I've wanted to use 7822 with a continuous crystal oscillator for clock (50% duty cycle) and I am trying to compute for the frequency to achieve a little more than 1.5MSPS (my signal is 750kHz). I need a continuous ADC and the 1µs power up time (if it powered down during the signal) will mean that AD 7822 is not for the job.

Thank you very much.


ps. I will use ad 7822 with arduino.

ad7822.pdf
Parents
  • Hi Mike3886,

       Figuring the set up, this may work, but please take note at 560ns period for the CONSVT, there will be exactly  30ns between the RD rising edge and the next CONVST falling edge (T3), which is very tight. Please make sure that this timing is met always during the conversion. Some deviation may affect the conversion process.

    Regards,

    Jonathan

Reply
  • Hi Mike3886,

       Figuring the set up, this may work, but please take note at 560ns period for the CONSVT, there will be exactly  30ns between the RD rising edge and the next CONVST falling edge (T3), which is very tight. Please make sure that this timing is met always during the conversion. Some deviation may affect the conversion process.

    Regards,

    Jonathan

Children
No Data