AD7616 : SE or differential input

Hi,

I have a question.

 

Is this device fully differential input possible or SE only?

The PIN description seems to SE only.

Our customer's circuit can be simplified If differential is possible.

 

Best regards,

Hiroshi

 

 

Parents
  • 0
    •  Analog Employees 
    on Sep 6, 2017 11:08 PM

    Hi Hiroshi,

       

       The AD7616 is a SE input. But if you are looking for a differential bipolar input, I can refer you to AD7609. It is an 8 channel 18 bit Bipolar ADC. Do you have a specific feature that you are looking for an ADC? By the way , what application you are planning to build?

    Regards,

    Jonathan

Reply
  • 0
    •  Analog Employees 
    on Sep 6, 2017 11:08 PM

    Hi Hiroshi,

       

       The AD7616 is a SE input. But if you are looking for a differential bipolar input, I can refer you to AD7609. It is an 8 channel 18 bit Bipolar ADC. Do you have a specific feature that you are looking for an ADC? By the way , what application you are planning to build?

    Regards,

    Jonathan

Children