AD7658 output comnparison problem

Hi all,

I'm using ad7658 in parallel mode. I have written my own fpga code to read the analog inputs. In simulation it works regularly but i can't see the true results at the outputs when i change it input voltage value.

In oscilloscope, the busy, cs and read signals are shown look like the simulation and true but i can't read the analog inputs. D0-D11 data aren't high z or zero, there are some values on the way. The real problem is when i change the input data up or down to 1V, there isn't any value change. The board İ have worked hasnt any uart output or sth like that so i canT observe the full data value at the same time because of this reason I preffered the comparision method.

Thnak you 

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;

entity main is
Port ( clk : in STD_LOGIC; --50MHz=20ns
analog_bus : in STD_LOGIC_VECTOR (15 downto 0); --default 16 bit fakat an7658 resolution [11:0]
busy : in STD_LOGIC; --analog to digital işleminin dönüştrülmesi için gerken süre min=3us
stby : out STD_LOGIC;

led : out STD_LOGIC_VECTOR (5 downto 0);
led_b : out STD_LOGIC_VECTOR (5 downto 0);
convst_a : out STD_LOGIC; --V1 and V2
convst_b : out STD_LOGIC; --V3 and V4
convst_c : out STD_LOGIC; --V5 and V6
cs : out STD_LOGIC; --veri aktarımı sırasında 0 olmalı
rd : out STD_LOGIC; --veri aktarımı sırasında 0 olmalı
reset : out STD_LOGIC); -- veri aktarımı sırasında reset=0 olmalı

end main;

architecture Behavioral of main is
--default values
signal stby_l : STD_LOGIC := '1';
signal convst_a_l : STD_LOGIC := '1';
signal convst_b_l : STD_LOGIC := '1';
signal convst_c_l : STD_LOGIC := '1';
signal cs_l : STD_LOGIC := '1';
signal rd_l : STD_LOGIC := '1';
signal reset_l : STD_LOGIC := '1';
signal V1 : STD_LOGIC_VECTOR (11 downto 0) := "000000000000";
signal V2 : STD_LOGIC_VECTOR (11 downto 0) := "000000000000";
signal V3 : STD_LOGIC_VECTOR (11 downto 0) := "000000000000";
signal V4 : STD_LOGIC_VECTOR (11 downto 0) := "000000000000";
signal V5 : STD_LOGIC_VECTOR (11 downto 0) := "000000000000";
signal V6 : STD_LOGIC_VECTOR (11 downto 0) := "000000000000";
signal cnt : integer range 0 to 16_777_215 ;
signal min : integer range 0 to 16_777_215 :=0;
signal busy_l : STD_LOGIC ;


type state_type is (Start_State,Wait_State, conv_a, conv_b, conv_c);
signal state : state_type := Start_State;

begin
process(clk)
begin
if(rising_edge(CLK)) then
case state is
when Start_State =>
min<= min+1;
stby_l <= '1';
if(min=0) then
reset_l <= '1';
end if;
if(min=5) then
reset_l <= '0';
convst_a_l <= '0';
convst_b_l <= '0';
convst_c_l <= '0';
state <= Wait_State;
min<=0;

end if;


when Wait_State =>
min<= min+1;
cs_l <= '1';
rd_l <='1';
if(min=50) then
convst_a_l <= '1';
convst_b_l <= '1';
convst_c_l <= '1';
end if;
if(convst_a_l='1' or convst_b_l='1' or convst_c_l='1') then
if(cnt=145) then
state <= conv_a;
cnt<=0;
cs_l<='0';
rd_l <= '0';
min<=0;
end if;
end if;

when conv_a => --convert v1 and v2
if(convst_a_l = '1') then
if(cnt=0 or cnt=1 or cnt=2 )then
rd_l <= '0';
v1<=analog_bus(11 downto 0);-- read v1 data
cnt <= cnt+1;
elsif( cnt = 3 or cnt=4 )then
rd_l <= '1';
cnt <= cnt+1;
elsif(cnt=5 or cnt = 6 or cnt=7 or cnt=8)then
rd_l <= '0';
v2<=analog_bus(11 downto 0);--read v2 data
cnt <= cnt+1;
elsif(cnt = 9 or cnt = 10 )then
rd_l <= '1';
cnt <= cnt+1;
elsif(cnt = 11)then
rd_l <= '0';
cnt <= 0;
state <= conv_b;
end if;
else
state <= conv_b;
end if;

when conv_b => --convert v3 and v4
if(convst_b_l = '1') then
if(cnt<3)then
rd_l <= '0';
v3<=analog_bus(11 downto 0);--read v3 data
cnt <= cnt+1;
elsif(cnt=3 or cnt=4)then
rd_l <= '1';
cnt <= cnt+1;
elsif(cnt = 5 or cnt=6 or cnt=7 or cnt = 8)then
rd_l <= '0';
v4<=analog_bus(11 downto 0);--read v4 data
cnt <= cnt+1;
elsif(cnt=9 or cnt = 10)then
rd_l <= '1';
cnt <= cnt+1;
elsif(cnt = 11)then
rd_l <= '0';
cnt <= 0;
state <= conv_c;
end if;
else
state <= conv_c;
end if;

when conv_c => --convert v5 and v6
if(convst_c_l = '1') then
if(cnt<3)then
rd_l <= '0';
v5<=analog_bus(11 downto 0);--read v5 data
cnt <= cnt+1;
elsif(cnt=3 or cnt=4)then
rd_l <= '1';
cnt <= cnt+1;
elsif(cnt=5 or cnt=6 or cnt=7 or cnt=8)then
rd_l <= '0';
v6<=analog_bus(11 downto 0);--read v6 data
cnt <= cnt+1;
elsif(cnt=9 or cnt = 10)then
rd_l <= '1';
cnt <= cnt+1;
elsif(cnt = 11)then
rd_l <= '1';
cnt <= 0;
state <= Wait_State;
cs_l <='1';
convst_a_l<='0';
convst_b_l<='0';
convst_c_l<='0';
end if;
else
state <= Wait_State;
cs_l <= '1';
rd_l <='1';
convst_a_l<='0';
convst_b_l<='0';
convst_c_l<='0';
end if;

end case;

end if;

end process;
busy_l<=busy;


led(0) <= not busy_l ;--3V
led(1) <= not cs_l ;--3V
led(2) <= not rd_l ;--3V

led(3) <= '0' when (v4>"000011001101") else '1';--1V
led(4) <= '0' when (v5>"000011001101") else '1';--1V
led(5) <= '0' when (v6>"000011001101") else '1';--1V

led_b(0) <= '0' when (v1>"000011001101") else '1';--1V
led_b(1) <= '0' when (v2>"000011001101") else '1';--1V
led_b(2) <= '0' when (v3>"000011001101") else '1';--1V
led_b(3) <= '0' when (v4>"000011001101") else '1';--1V
led_b(4) <= '0' when (v5>"000011001101") else '1';--1V
led_b(5) <= '0' when (v6>"000011001101") else '1';--1V


convst_a <= convst_a_l ;
convst_b <= convst_b_l ;
convst_c <= convst_c_l ;
cs <= cs_l ;
rd <= rd_l;
reset <= reset_l;
stby <= stby_l;

end Behavioral;

  • 0
    •  Analog Employees 
    on Sep 8, 2017 1:02 AM

    Hi Herdinc,

       If it is possible, can you share the schematic of the application, I can have a better understanding of the possible situation. Please also check on the voltage level of the supplies AVcc, Vdd, DVcc and Vdrive of the set up make sure that they are in correct and recommended in the datasheet.

    Regards,

    Jonathan

  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:56 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin