Post Go back to editing

Generating common mode voltage for AD779x

Hello,

I am asking advice in the following issue.

I want to sample the output of a ADA4530-1 ( TIA configuration ) with an AD7793 ADC.

Since I want to use the internal INA of the AD7793 I need to bias the input to shift it to an

acceptable common mode range.

So far I have used an THS4521 differential amplifier to generate a biased common voltage

signal but I was wondering if there is a better way to accomplish this _without_ the use of an extra opamp.

If a single-to-differential opamp is required, what would be the best choice for a precision, low bandwidth

part from ADI. ( ADA4941-1 ? )

Thank you very much!
Peter

  • Hi,

      I'll get back to you soon. I am looking in to this.

    Thanks,

    Jellenie

  • Hi,

    Regarding the selection of single to differential amplifier, I think someone from the ADC Drivers community might be able to help you. However, can you provide us more details regarding your target application? May I know also what is your input range and what supply voltage you want to operate? If you could also send us the schematic diagram, it would be great. 

    Thanks,

    Jellenie

  • Hi Jellenie,

    thanks for the reply!

    > can you provide us more details regarding  your target application?

    I need to readout a photodiode for ultra low light intensities

    > May I know also what is your input range and

    the output of the ada4530-1 is only a few 10 mV

    > what supply voltage you want to operate?

    Supply voltage is 3.3V

    Again, the general question is how to provide the required common mode

    voltage (mid-supply) for the internal instrumentation of the AD7793

    without the use of an additional single-ended->differential opamp.

    Could well be that there is no way around to using that extra amplifier ....

    Thanks

    Peter

    Am 20.09.2017 um 10:39 schrieb JellenieR:

      EngineerZone <https://ez.analog.com/?et=watches.email.thread>

        Re: Generating common mode voltage for AD779x

    reply from JellenieR

    <> in

    /Precision ADCs/ - View the full discussion

    <https://ez.analog.com/message/318467?commentID=318467&et=watches.email.thread#comment-318467>

    >

  • Hi,

    There's a restriction on the analog input range and common mode voltage when the in-amp is active. This will really requires you an analog front end to ensure that the limits are not exceeded for correct operation and to avoid linearity performance. So if your input is around 10mV, the negative input should be bias to at least 1V to meet the common mode requirements.

    Would you like to consider using the AD7124, it has all the building blocks of the AD7793 with some advanced features. In AD7124, the common mode range must be between (AVSS − 0.05 + 0.5/gain) and (AVDD − 0.1 − 0.5/gain). The part can also accept a pseudo differential input so it can operate in a single ended application as it has a flexible MUX in which any analog of the analog input pins can be positive or negative input. So, in your application you can connect your single ended input to the one of the positive input and you can use the bias voltage midway between the analog power supply rails generated internally as your negative input. This generated bias voltage can be made available at any VBIAS pins and you can connect this to your selected negative input.

    Thanks,

    Jellenie

  • Hi Jellenie,

    thank you very much for taking the time to answer my question.

    I appreciate!

    The AD7124 looks like a good part to solve my goal to omit the

    extra opamp. I will look into your suggested solution.

    Best regards

    Peter

    Am 25.09.2017 um 04:46 schrieb JellenieR:

      EngineerZone <https://ez.analog.com/?et=watches.email.thread>

        Re: Generating common mode voltage for AD779x

    reply from JellenieR

    <> in

    /Precision ADCs/ - View the full discussion

    <https://ez.analog.com/message/319070?commentID=319070&et=watches.email.thread#comment-319070>

    >

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin