Post Go back to editing

AD7761 Throughput and Dclk

Hey everyone,

I have a quick question on the Dclk of the AD7761,On page 45 of the datasheet, It states the minimum Dclk configuration that can be used is dependent on the throughput and channels per Doutx.

I'll be using a daisy chain configuration of three devices (so 2 output lines) and I plan on having a dataoutput rate of 16Khz ( as defined in table 10/11 on page 28).

So my minimum Dclk should be = 16ksPs * 2 channels * 24 = 768 kHz, but it seems the Dclk division can only be a minimum of Mclk/8 and Mclk needs to be 32.768 Mhz, so this equates to 4.096 MHz, which is a lot higher than my required Dclk. Is there any way that I can get the Dclk closer to 800 kHz? It'll be easier on my processor to process the incoming data if it comes out close to 800 kHz instead of 4MHz

Thanks in advance for any help.

  • Hi,

    There are a number of factors to consider in order to calculate the minimum DCLK rate. The first point I would make is that MCLK does not have to be a fixed 32.768MHz. 32MHz is the MCLK needed to achieve the highest output data rate (ODR). Assuming you want the lowest power solution for daisy chaining 3 devices, assuming 2 DOUTs in use, I would calculate it as follows:

    • Minimum DCLK needed is - 16,000 samples x 24 bits per conversion x 4 channels per DOUT x 3 devices = 4.608MHz minimum.
    • Lowest MCLK possible is - 16kSPS x 32 (for decimation) x 32 (for internal clock divider, low power mode) = 16.384MHz.
    • The DCLK divide option needed is DCLK/2 since DCLK/4 does not meet the 4.608MHz requirement.
    • Fmod remains within the recommended rate of 0.036 to 1.024 MHz for low power mode.

    The Pin Control settings would then be set as follows:

    Dec1      0

    Dec0      0

    Mode3    0

    Mode2    0

    Mode1    0

    Mode0    1

    You also have the option to select either a sinc or wideband filter. If a higher performance configuration is needed this is also possible at the expense of burning more power by changing power modes. You could also use a 32.768MHz MCLK and decimate by 64 rather than 32 for greater performance

    Regards

    Niall

  • Thank you NiallM, this completely solves this.