Development board for AD7124-4

Hi,

I was wondering if there was a development board for the AD7124-4. The evaluation kit EVAL-AD7124-4SDZ, but I can't seem to access the MISO, MOSI, SCK, CS lines (or am I missing something?). I'm primarily looking for writing a driver for my AD7124-4 and I want to test it on a vendor provided board first. 

Parents
  • 0
    •  Analog Employees 
    on Nov 9, 2017 6:13 PM

    Hi, Jay.

    Apologize. I have edited the link page.

    1. Yes, to operate the EVAL-AD7124-4SDZ in standalone mode, the AD7124-4 serial interface lines can be disconnected from the 120-pin header by removing the 0 Ω links, R9 through R13. The test points can then be used to connect it to other controller. 

    2. You can use the driver as it is for AD7124 configuration. However, the actual SPI communication settings or functions will depends on the desired type of processor and communication protocol.

    Thanks,

    Jellenie

Reply
  • 0
    •  Analog Employees 
    on Nov 9, 2017 6:13 PM

    Hi, Jay.

    Apologize. I have edited the link page.

    1. Yes, to operate the EVAL-AD7124-4SDZ in standalone mode, the AD7124-4 serial interface lines can be disconnected from the 120-pin header by removing the 0 Ω links, R9 through R13. The test points can then be used to connect it to other controller. 

    2. You can use the driver as it is for AD7124 configuration. However, the actual SPI communication settings or functions will depends on the desired type of processor and communication protocol.

    Thanks,

    Jellenie

Children
No Data