Post Go back to editing

AD7171 output data rate variations

Hi,

I have a question about AD7171.

Q :  Is the data rate in the range of 125Hz +/- 10%?

 

According to D/S, 125Hz 「TYP」

Because customer apps is real time temp sensing, they needs variation specs.  

And, the user must ensure that the complete word is read before the next conversion is complete.

I think that large variations make design impossible...

Fortunately the internal clock is +/- 5% max/min , so I think that it is not so large variations.

 

Best regards,

Hiroshi