adcs

I require an adc with 40 channel ,16 bit and 300KSPS to 1msps speed and 40 channel can be from 2 or 3 adcs but with 16 bit and 300ksps to 1msps speed and should have synchronization pin to have synchronization operation for all adcs.

  • 0
    •  Analog Employees 
    on Feb 13, 2018 12:30 AM over 2 years ago

    Hi,

       Do you have a bandwidth requirement of the ADC? You can check ADAS3023 AD7768 AD7616. The AD7768 has synchronization feature to synchronize all the ADC connected from the same MCLK. You can check details in ADI website http://www.analog.com/en/parametricsearch/10994#/p1746=16.6|10000000&p4369=Simultaneous%20Sampling&p3062=|3|4|5|6|7|8|10|12|16&p193=16|18|24

  • I require an adc with 16 bit with sync pin to synchronize and speed of min

    300ksps and minimum of 8 channel adc

    On Tue, Feb 13, 2018 at 2:01 PM, jcolao <

  • 0
    •  Analog Employees 
    on Feb 26, 2018 3:50 AM over 2 years ago

    Hi,

       I can recommend to you the two ADCs. The AD7616 and AD7768. They have different architecture, the AD7616 is a SAR and AD7768 is a Sigma Delta. The AD7616 is a 16bit , 16 channel dual simultaneous sampling ADC and has a throughput rate of 1MSPS. The sampling can be synchronize using the CONVST pins. Another ADC that I would recommend is the AD7768, which I think very close to what you are looking for. The AD7768 is a 24bit , 256ksps output data rate. The AD7768 can sample 8 channels at the same time. The AD7768 has a synchronization pins to allow  multiple AD7768 connected attune from a single master clock. You can refer to the links of the datasheet of these ADCs. 

    Regards,

    Jonathan

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:02 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin