Post Go back to editing

LTC1856 configuring and reading back differential channels

I'm testing the LTC1856 differential channels, Chan 6 & 7. I'm confused how to configure them and read them back.

Both channels work in single ended mode reading back 32767 0x7FFF with +10V input.

When I configure the channels as differential and input +10V on chan 6 and -10V on chan 7 I read back 32767 from both channels. I also get the same result when injecting +5V on chan 6 and -5V on chan 7?

I've configured both channels with the input word 00110000 which should configure the multiplexer for differential channels + on 6 and - on 7.

Parents
  • Hello  and ,

    Thanks for your reply. Yes BBB has SPI port so we will use SPI port for communication between LTC1856  and BBB

    We have study LTC1856 datasheet and found that this works on 5V and BBB SPI port work on 3.3V.

    So is there any level sifter required ?

    Can we directly connect BBB SPI port with LTC1856 ?

Reply
  • Hello  and ,

    Thanks for your reply. Yes BBB has SPI port so we will use SPI port for communication between LTC1856  and BBB

    We have study LTC1856 datasheet and found that this works on 5V and BBB SPI port work on 3.3V.

    So is there any level sifter required ?

    Can we directly connect BBB SPI port with LTC1856 ?

Children
No Data