I'm testing the LTC1856 differential channels, Chan 6 & 7. I'm confused how to configure them and read them back.
Both channels work in single ended mode reading back 32767 0x7FFF with +10V input.
When I configure the channels as differential and input +10V on chan 6 and -10V on chan 7 I read back 32767 from both channels. I also get the same result when injecting +5V on chan 6 and -5V on chan 7?
I've configured both channels with the input word 00110000 which should configure the multiplexer for differential channels + on 6 and - on 7.