Post Go back to editing

I am searching for a very low consumption 16bit ADC capable of 0-5V input, 100 Sps, 8 Channels high impedance input

It seems to be that this is not possible to find in one chip.
I found ADAS3022 which has 8 inputs high impedance, 0-5V and 0-10V input 16bit. But this consumes quite much current.

I also found AD7171 which is low power but needs external reference 5V for 0-5V, external MUX and may be external buffer for high impedance.
I know that there were multimeter circuits like ICL7109 which had very high input impedance, stable values, but unfortunately no 0-5V input and no multiplexer in front.

I would need a solution for a data logger - battery driven - and therefore need something with very small current consumption that does not need to be very fast. 100 Sps or so would be ok.

May be somebody has an idea.

Thank you very much !

  • Hi Matt,

    ADAS3022 is not a good choice since it requires dual supply which is not applicable in battery-operated application. Thus, I suggest you to use AD7689, a 16-bit, 8-channel, 250ksps PulSAR ADCs. It contains 16-bit ADC, 8-channel low crosstalk multiplexer, an internal low  drift reference and buffer, temperature sensor and sequencer. But this requires external 8 ADC driver. You can use ADA4805 or ADA4807 as driver. For reference, you can utilize the internal reference of 2.5V or 4.096V but still you can use external reference of 5V using voltage reference like ADR4550 and the internal buffer.

    By the Way, may I know your supply voltage for this application.

    Regards,

    Daryl

  • Thank you Daryl,
    the supply voltage is not so sure at the moment. May be there will be 3.3V and 5V. 
    Thank you for the hint to the AD7689. I will have a look at the data sheet.
    8 external OP amps are possible - but this takes quite some space for all those and may be as well the series resistors and caps according to the data sheet http://www.analog.com/media/en/technical-documentation/data-sheets/ADA4805-1_4805-2.pdf. The offset may differ from channel to channel then. 125uV means some LSBs. Using 5V as supply may be some upper bits are lost or the op amps would have to be supplied by 5.5V or so. When using the ADR4550 with 300mV drop also the 5.5V could do.
    Another possibility would be using an external MUX like DG406 and a buffer amp after this in front of the ADC. Using this only one amp would be necessary. Also using a divider up to 10V also would be possible.

    Regards,
    Matthias

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.