Post Go back to editing

Differential input to ADC IN+ and ADC- for DC2390A Evaluation board

Hi,

I'm a bit stumped at the moment with my measurements on the DC2390A board. According to the LTC2500-32 data sheet, IN+ and IN- accepts between 0-5V.

I'm operating the evaluation board in differential mode (ie CH1_1 and CH1_2 as well as CH2_1 and CH2_2 with all the recommended components additions and subtractions). 

The front end amplifiers LT1468 specs for the board say "+/-10V" signal range. So working out the math/analysis with DC constant voltage at +10V and -10V at input, and working out the voltages down to the ADC IN+ and ADC IN- pins on U2, I would see ADC IN+ seeing +7.5V and ADC IN- seeing -2.5V. U20 output is balancing at 5V.

However, LTC2500-32 data sheets specifies IN+ and IN- voltages to be between 0V - 5V. This would mean at +/-10V, the signal is being clamped.

I'm currently seeing saturation in my bit output and would like to double check if my calculations are correct and that the board wasn't set up correctly for +/-10V(?). 

Much appreciated,


R.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.