I am using AD7091r_2, using REF198 as thethe refered voltage,which is 4.096V , and the input voltage of Vin0 and Vin1 of the AD7091r_2 is from 0 to 6V , when the input of Vin0 is 6V and the input of Vin1 is 0V, the REF IN/REF OUT pin of AD7091r_2 become 6V . When the REF IN/REF OUT pin of AD7091r_2 is disconnected , the REF IN/REF OUT pin is still 6.0V when the input of Vin0 is 6V and the input of Vin1 is 0V, what is happening ?
or the input of the Vin0 and Vin1 must be controled beside the refered voltage 4.096V ?
Edit Notes
add description of the REF IN/REF OUT pin of AD7091r_2[edited by: microchip_zh at 10:02 PM (GMT 0) on 10 Jun 2020]