Post Go back to editing

BIA measurements with AD5941

Thread Summary

The user is attempting to measure resistances between 10 ohms and 10 kohms using the EVAL-AD5941ARDZ and SensorPal software for a university project. The EVAL-AD5941ARDZ is not suitable for BIA measurements due to missing protection components and incorrect connections. However, the user can measure resistance values using the Impedance measurement mode in SensorPal after setting switches JP10 and JP11 to position C.
AI Generated Content

Hi, everybody,

I am doing a project for the university and need to do BIA test measurements with AD5941 and EVAL AD5941ARDZ. For this I have to measure different resistances of values between 10 ohms and 10 kohms at different frequencies.

I have been looking at the user guide of the AD594x and I have found examples to make the measurements but I have followed the steps and I have not obtained the expected results.

If I use the SensorPal software, how should I connect the 4 wires (red, black, blue and green) to the resistance and what parameters should I modify in the application?

And if I use other software such as Keil + Realterm, how should I connect the 4 wires and what code parameters in Keil should I modify in order to make the measurements?

Thank you very much!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.