AD776
Obsolete
The AD776 is a 16-bit sigma-delta oversampled ADC, incorporating a 1-bit third-order modulator and digital decimation filter. An on-chip voltage reference...
AD776 on Analog.com
AD7767
Production
The AD7767/AD7767-1/AD7767-2 are high performance, 24-bit, oversampled SAR analog-to-digital converters (ADCs). The AD7767/AD7767-1/AD7767-2 combine the...
Datasheet
AD7767 on Analog.com
AD7765
Production
The AD7765 is a high performance, 24-bit sigma-delta (S-?) analog-to-digital converter (ADC). It combines wide input bandwidth, high speed, and performance...
Datasheet
AD7765 on Analog.com
AD7766
Production
The AD7766/AD7766-1/AD7766-2 are high performance,
24-bit, oversampled SAR analog-to-digital converters (ADCs).
The AD7766/AD7766-1/AD7766-2 combine the...
Datasheet
AD7766 on Analog.com
I would like to interface a photodiode transimpedance amplifier to a 24bit ADC (AD7765, AD776, AD7767 or similar). The largest source of error appears to be the drift of the transimpedance amp (TIA), rather than noise.
We prefer to use a linear amplifier, rather than a logarithmic amplifier. The topology is thus a linear TIA followed by either by a single ended to differential amp stage or by grounding one side of the ADC input if it provides better performance.
Assuming a 40 degree change in temperature, a 0.5uV/degree offset coefficient leads to a 20 uV input. If both the TIA and the SE to DE stage have a 0.5uV/degree drift coefficient, total drift could be as large as 40uV, which is too big for our application. For comparison a TIA gain of 5K in a 25kHz bandwidth has less than 2uV RMS noise, using a low noise TIA.
I would very much appreciate recommendations for TIA amplifiers, single-ended to differential amp, and input topology for achieving the lowest possible total error, within a -5 to 65 degree temperature range.
System parameters are:
Photocurrent range: 20nA to 1mA
Sampling rate: approximately 30 to 50 kilosamples/sec
Photodiode capacitance: 10pF
Thanks
Bernard Harris
Hi-
I moved this discussion to the Amplifiers Community. Someone here should be able to assist you.
Regards,
AndyR
EngineerZone Community Manager
Hi-
I moved this discussion to the Amplifiers Community. Someone here should be able to assist you.
Regards,
AndyR
EngineerZone Community Manager