AD776
Obsolete
The AD776 is a 16-bit sigma-delta oversampled ADC, incorporating a 1-bit third-order modulator and digital decimation filter. An on-chip voltage reference...
AD776 on Analog.com
AD7767
Production
The AD7767/AD7767-1/AD7767-2 are high performance, 24-bit, oversampled SAR analog-to-digital converters (ADCs). The AD7767/AD7767-1/AD7767-2 combine the...
Datasheet
AD7767 on Analog.com
AD7765
Production
The AD7765 is a high performance, 24-bit sigma-delta (S-?) analog-to-digital converter (ADC). It combines wide input bandwidth, high speed, and performance...
Datasheet
AD7765 on Analog.com
AD7766
Production
The AD7766/AD7766-1/AD7766-2 are high performance,
24-bit, oversampled SAR analog-to-digital converters (ADCs).
The AD7766/AD7766-1/AD7766-2 combine the...
Datasheet
AD7766 on Analog.com
I would like to interface a photodiode transimpedance amplifier to a 24bit ADC (AD7765, AD776, AD7767 or similar). The largest source of error appears to be the drift of the transimpedance amp (TIA), rather than noise.
We prefer to use a linear amplifier, rather than a logarithmic amplifier. The topology is thus a linear TIA followed by either by a single ended to differential amp stage or by grounding one side of the ADC input if it provides better performance.
Assuming a 40 degree change in temperature, a 0.5uV/degree offset coefficient leads to a 20 uV input. If both the TIA and the SE to DE stage have a 0.5uV/degree drift coefficient, total drift could be as large as 40uV, which is too big for our application. For comparison a TIA gain of 5K in a 25kHz bandwidth has less than 2uV RMS noise, using a low noise TIA.
I would very much appreciate recommendations for TIA amplifiers, single-ended to differential amp, and input topology for achieving the lowest possible total error, within a -5 to 65 degree temperature range.
System parameters are:
Photocurrent range: 20nA to 1mA
Sampling rate: approximately 30 to 50 kilosamples/sec
Photodiode capacitance: 10pF
Thanks
Bernard Harris
Hi Bernhard,
I'll get some recommendations on the amplifier stages from my colleagues in the amplifier division of Analog Devices and we can get some cct diagrams together for you to look at.
Regards,
Michael.
Hi Bernhard,
I'll get some recommendations on the amplifier stages from my colleagues in the amplifier division of Analog Devices and we can get some cct diagrams together for you to look at.
Regards,
Michael.