Post Go back to editing

SPI interface for AD4020

Hello,

I have been using the AD4020 eval board for a few months now. I am very satisfied with what the ADC has to offer. However for my future needs I have to integrate it into my existing PCB. The hardware for this is pretty much open source and I was able to decide on a minimalistic version of the eval board. However, the SPI interface isn't available for this. Has anyone tried to write SPI driver to read and get the data out of the ADC in either C or python? I am in a bit of a time crunch, so I can't afford to write it from scratch as of now. Any base code or pointers would really help.

The SBC I am using currently is the beaglebone black. So any C code or python code would help me get a quick start.

Regards

Mohan Prabhakar 



Added tags for internal tracking purposes
[edited by: tschmitt at 1:27 PM (GMT 0) on 24 Feb 2020]
Parents Reply Children
No Data