Question: How can I tell that the model part is a standard silicon or B-grade?
AD7124-8
Recommended for New Designs
The AD7124-8 is a low power, low noise, completely integrated
analog front end for high precision measurement applications. The
AD7124-8 W grade is AEC...
Datasheet
AD7124-8 on Analog.com
AD7124-4
Recommended for New Designs
The AD7124-4 is a low power, low noise, completely integrated analog front end for high precision measurement applications. The device contains a low noise...
Datasheet
AD7124-4 on Analog.com
Question: How can I tell that the model part is a standard silicon or B-grade?
When ordering there are two options available, AD7124-4BBCPZ/AD7124-8BBCPZ-RL and AD7124-4BCPZ/AD7124-8BCPZ-RL. The extra B in the first option represent the B-grade. The B-grade offers substantial improvement over the standard silicon and therefore would be recommended for new design, for full details on the differences see link below:
When ordering there are two options available, AD7124-4BBCPZ/AD7124-8BBCPZ-RL and AD7124-4BCPZ/AD7124-8BCPZ-RL. The extra B in the first option represent the B-grade. The B-grade offers substantial improvement over the standard silicon and therefore would be recommended for new design, for full details on the differences see link below: