Hi,
I would like to use the AD5940 chip with a custom design in order to provide pH measures on water. To achieve this, I ported the ad5940lib to our MCU to communicate with the chip through SPI and I successfully run the examples on the ad5940-examples repository.
To evaluate the capability of the AD5940 chip to perform pH measures, I previously tested the EVAL-CN0428-EBZ board with the "Water Quality" example and I obtained satisfactory results.
Now, I would like to port this example to our platform with the AD5940 chip (preferably using the ad5940lib) but I found some difficulties in this process, in particular:
- The EVAL-CN0428-EBZ uses the ADuCM355 instead of the AD5940 and the API used to configure the chip is completely different respect to the ad5940lib;
- The repository aducm355-examples is still empty, so I can make no comparison with the configuration of the ADuCM355 using the ad5940lib;
- I can't see any useful example in the ad5940-examples repository to perform pH measures;
Is there any possibility to get the pH measure example ported to the ad5940lib? If not, do you suggest to implement the application using the ad5940lib anyway or do you think there is a simpler approach to get the example work?
Thank you.