Hi, I have a problem with ADA3023 since I cannot read the conversion with a dPIC, first of all the first thing I have done is the following check:
there is a voltage of 5V and + -15V. In the ACAP PIN, RCAP and REFIN there are 2.5V and in REF1.2 = 4.096V, I have left the default CFFF register FFFF and use the datasheet initialization sequence for the power supply.
After these checks I have done the ADC readings by the sPI and they fluctuated. After analyzing with the oscilloscope I have noticed that the BUsY PIN does not change, it is always at zero it does not warn that the conversion is finished. I have changed the ADA3023 for two times for a new one, assuming this was a problem but the PIN BUsY remains the same.
I don't know what else I can do!
thanks!
Adding Tags
[edited by: @skowalik at 6:39 PM (GMT 0) on 29 Dec 2019]