AD2S1205 startup issue

Hello, I'm testing a new design with a AD2S1205 resolver decoder. I have my design assembled, and applied 5v to the Vdd. I have been using a 100 ohm resistor to pull down the reset signal by hand, and when I remove it I observe the current draw by the 5v rail to go from <10mA to >10mA, so I believe that to be working. In addition, I see the voltage at EXC and !EXC as well as the clock input go from 0v to ~2.5v. However, I can't seem to find any other indication that the AD2S1205 is operational. I assume that the complimentary EXC signals should be generating a 10khz signal, and that the IC should be trying to oscillate the 8.192mhz crystal, but neither seems to be the case.

I suspected that the IC was damaged, and replaced it with a new one, but the new one behaves the same way.

What behavior should I look for to indicate that the device works? What do I need to do to get the IC to excite the resolver coils?