for AD7321 when it is single-ended mode, the output is 12bits,
My concern is when in single-ended mode, which bits are useful in the first figure? sign bit + DB11-DB1 or DB11-DB0?
Looking forward to your answer.
Thank you very much!
AD7321
Production
The AD7321 is a 2-channel, 12-bit plus sign successive approximation ADC designed on the iCMOS (industrial CMOS) process. iCMOS is a process combining...
Datasheet
AD7321 on Analog.com
for AD7321 when it is single-ended mode, the output is 12bits,
My concern is when in single-ended mode, which bits are useful in the first figure? sign bit + DB11-DB1 or DB11-DB0?
Looking forward to your answer.
Thank you very much!
Maggie,
The product support representative for the AD7321 is out of the office until January 6, 2020 as all ADI offices are closed until that date. They will be better equipped to answer your question upon their return. I apologize for any inconvenience this delay will cause.
Sean
Hi, Do you now have some one to answer this? thanks!
Maggie,
My apologies that you have not received a response with regards to you inquiry to this point. I will escalate the query again to see if I can't get you an answer.
Sean
Hi Maggie,
The 13th "bit" in single-ended/pseudo diff mode is just noise, and can be discarded. This is the LSB on the diagram.
Is there a specific issue that you see when you are reading the data back in your application? What processor are you using to interface to the AD7321?
Regards,
Hein
Hi Maggie,
The 13th "bit" in single-ended/pseudo diff mode is just noise, and can be discarded. This is the LSB on the diagram.
Is there a specific issue that you see when you are reading the data back in your application? What processor are you using to interface to the AD7321?
Regards,
Hein
Thanks !
I got it.
I am planning to use it right now and it is our candidate.